Part Number: TLV8541
Other Parts Discussed in Thread: CC1310, TPS22860,
Hi,
My customer is developing a wireless system where they use micro CC1310 and CC2642 + TLV71318, TPS22860, TPS619291 and TLV8541.
For cost optimization, I was considering whether to add protections to the non-inverting input of the TLV8541DBVR.
We are currently using it in a Non-inverting configuration with input impedance of several MegaOhm. I wanted to ask if the operational input has diodes that can act as a clamp in case the input voltage exceeds the operating range provided by the integrated for a few moments ... or should the input be protected with external clamp diodes?
Ex: TLV8541DBVR powered at 3V. Non-inverting input with 2MOhm series resistance: it is essential to put clamp diodes on the input (e.g. BAV199) to protect the operational input from overvoltages (e.g. -50V or + 50V) or I can consider that, given the high input impedances, the operational is not damaged?
Please let me know,
Many Thanks,
Antonio