Part Number: AMC3301
Hi,
As the datasheet, AMC3301 should be used in single ended mode: connecting negative input (INN) to floating ground (HGND). I am wondered if it is possible to operate the device input in fully differential mode as long as the input common mode range is maintained? (-0.16V to 1V)
The reason why asking this question is i am proposing customer to measure high DC voltage (+/-1kV) with this device. Considering the high resistance divider is used, a buffer has to be used in front of AMC3301 to maintain accuracy. Since the buffer is powered from single polar supply (HLDOout), to achieve +/-1000V input range the device has to be operated in fully differential mode.
Thank you,
John