Part Number: LM111QML
Tool/software: WEBENCH® Design Tools
Can you share me LM111QML spice model?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Here is what is in the TINA V11 library, also a .txt file of the model listing, you can perhaps use this get to your desired model file.
*$ *////////////////////////////////////////////////////////////////////// * (C) National Semiconductor, Inc. * Models developed and under copyright by: * National Semiconductor, Inc. *///////////////////////////////////////////////////////////////////// * Legal Notice: This material is intended for free software support. * The file may be copied, and distributed; however, reselling the * material is illegal* /////////////////////////////////////////////////////////////////// * For ordering or technical information on these models, contact: * National Semiconductor's Customer Response Center * 7:00 A.M.--7:00 P.M. U.S. Central Time * (800) 272-9959 * ///////////////////////////////////////// * LM111 Voltage Comparator * ///////////////////////////////////////// * * Connections: * Positive Input * | Negative Input * | | Positive power supply * | | | Negative Power supply * | | | | Output * | | | | | Ground or Emitter Output * | | | | | | .SUBCKT LM111 3 2 8 4 1 104 * * PINOUT ORDER +IN -IN V+ V- OUT GND * * CAUTION: SET .OPTIONS GMIN=1E-16 TO CORRECTLY MODEL INPUT BIAS CURRENT. * Features: * Operates from single 5V supply * Very Low Input current * Very Low Power Consumption * * NOTE: - Noise is not modeled. * - Asymmetrical gain is not modeled. * *----- input stage ----- vos 2 13 dc 0.0007 iee 8 10 dc 1e-4 rc_q1 11 4 1517.2 rc_q2 12 4 1517.2 re_q1 10 6 1000 re_q2 10 7 1000 q1 11 3 6 mq1 q2 12 13 7 mq2 *----- supply current ----- gsup 8 4 33 4 1 rsup 8 45 33333.3 dsup 45 4 mds iis 4 33 dc 0.00395 ris 33 4 1 TC=-0.00379747, -3.55271e-20 *----- delay vs. overdrive ----- g1 4 25 12 11 10 rcl 25 4 10 dcl1 25 26 md0 dcl2 27 25 md0 vcl1 26 4 dc 9.4 vcl2 4 27 dc 9.4 g2 4 16 25 4 0.01 d3 16 18 md1 d4 17 16 md1 v1 18 4 dc 0 v2 4 17 dc 0 *----- inter stage ----- gb 4 20 12 11 100 rb 20 4 10 h1 22 4 poly(1) v1 0 1089.83 -4491.35 h2 4 21 poly(1) v2 0 1089.83 -4491.35 db1 20 22 mdb1 db2 21 20 mdb1 gt 4 30 20 4 1e-5 rt 30 4 100k ct 30 4 0.8116e-12 gc 4 35 30 4 0.003448 rc 35 4 1k *----- output satge ----- go 104 40 35 4 -0.01 ro 104 40 10 eob 41 40 45 4 1 rr 1 104 1meg co 40 104 10p voe 42 104 dc -0.0477 qo 1 41 42 mqo .model mq1 pnp bf=805.452 xtb=1.1526 .model mq2 pnp bf=861.069 xtb=1.1526 .model md0 d is=1e-10 rs=0.01 .model md1 d is=1e-12 .model mdb1 d .model mds d is=1e-16 .model mqo npn bf=100 rc=13.4286 isc=1.8e-10 + br=10 nr=0.95 cjs=5p cjc=1p tf=2n .ENDS
Thanks Michael!
If you need any assistance with this, please let us know. You should be able to run the .txt file Michael shared and rename it as a .lib. You should then be able to import it into your mode editor where you can assign an appropriate library symbol to the macro.
Regards,
Jonny