Part Number: LM2901
Hi Team,
my customer is using LM2901 as comparator,
they wanted to set Vref=0.3 V , and if V+ higher than Vref than output will act as 1(high level) , V+ lower than Vref than output will act as 0(low level) , the Vin level will be 0~2V (analog input), Vsup will set as 3.3V.
just for quick check , above application is doable and correct is that right?
(the Vin might higher than VICR= 3.3-2=1.3V, but the Vref is been set as 0.3V , which is lower than VICR , so the device will act as customer require per check by d/s 9.2.2.1 . )
do let me know if there's any concern of this application, thanks!
Andy