This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
My customer is examining the application with GND connection like material attached.
Is it possible to use INA180-Q1 in such application circuit as long as VCM always meet the recommended range(-0.2v to 26v)?INA180-Q1 lowside sensing application-1.pptx
Regards,
H.Someno
Hi Someno-san,
It is OK, when the voltages at the two input pins are kept above -0.2V as specified in the datasheet.
Regards, Guang