The customer wants to confirm TLV4376 operational amplifier. ・ The input offset voltage is 125uV, The customer's understanding is this value is the maximum and negative side is up to -125uV even when a single 5V power supply is used. Is it correct? -When using the common mode in the data sheet, there is a description of the offset voltage of 2.5 mV, Do you agree that there is no possibility of swinging up to this point when using differential or buffering?
Regards,