Other Parts Discussed in Thread: ISO124
HI
I am using an ISO 124 based isolation amplifier in my signal conditioning chain. Just before iso amp there is a differential amplifier whose output is single ended. so effectively one input of iso 124 will be the signal and other( GND 1) will be chassis ground of previous amplifier. The output is connected to PXI based data acquisition system. My doubt is which is the best possible way to connect the shield of the output wire to DAQ...differential or single ended.
The length is 3metres. Two core shielded. What is the min possible peak t0 peak noise obtainable with the iso 124. I am using a sampling rate of 1000.