Other Parts Discussed in Thread: LM358, LM317, OPA2137, TL032, TL082, TL052, TL072
I am using LM358 as a difference amplifier with gain 10 and then the second one also as a difference op amp with gain 10. Vcc is 22.5V and Vee is 0v. Bypass caps = 0.1uF.
Circuit is wired on breadboard.
The difference amplifier is connected across a 0.1 ohm current sense resistor. The voltage across the sense resistor is 15mV, but the output of the difference amplifier is 830mV.
The resistors are 1% metal film. I don't understand why it's 830mV instead of 15mv*10=150mV.
Even if I consider 6mV offset voltage, the max output will be (15+6)*10 = 210mV.
I don't understand why I am getting 830mV?
Just to make sure the op amp isn't broke, I shorted the 2 input terminal to ground. The output was 0.2mV.
pdf of ckt attached.4382.Circuit5a opamp.pdf