Part Number: BOOSTXL-AFE031-DF1
Other Parts Discussed in Thread: AFE032, AFE031, , C2000WARE, TMS320F28379D, LAUNCHXL-F280049C
Hello.
I'm a developer working on a commercial product, and my boss asked me to evaluate if AFE031 (or AFE032) is a good choice for our newest project.
So, I ordered 2 sets of: C2000 Piccolo MCU F280049C LaunchPad and BOOSTXL-AFE031-DF1.
The problem is that the product that we want to use the AFE031 on uses a different processor (from ST), so, I need to estimate how difficult it would be to reverse-engineer the example code and port it to a different processor. I managed to figure out the transmission part, but on the receiving end, the main functionality is in a pre-compiled .lib file (\C2000Ware_2_01_00_00\device_support\f28004x\examples\boostxl_afe031_f28004x_rx\fsk_corr_detect.lib)
So, is there anywhere I can get the source-code for this file? Or should I just recommend my boss to pick a plc-frontend from a different manufacturer?