This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ500100: 30W wireless solution

Part Number: BQ500100
Other Parts Discussed in Thread: INA199, INA210

Hi team,

Do we have 30W wireless charging solution or roadmap? just want to make sure. Thank you very much!

George

  • George,

    We currently do not have a wireless charging solution on the current sensing roadmap.  However, we do see our INA199 and INA210 devices used here for protection, one example application is the detection of metal objects placed on the charging pad.

    If the INA199 or INA210 devices do not meet your requirements please email me the details on what you are trying to accomplish.  I will see if any of our existing devices could be a good fit.  Also I am willing to add any compelling idea to our creative backlog for future consideration.  

    Regards,

    Dennis