Part Number: INA219
Dear Team,
Can this device sense AC input voltage and AC input current?
If not, do you have a suitable solution in your product line?
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA219
Dear Team,
Can this device sense AC input voltage and AC input current?
If not, do you have a suitable solution in your product line?
BR
Kevin
Hi Kevin,
It can measure certain AC inputs, but not all.
It will be helpful if you could define the inputs with more details, through key parameters such as shape, amplitude, frequency and DC offset.
Regards, Guang
Dear Guang
It is for:
Sine wave
No DC offset
Voltage -> 97~264VAC
F = 47~63Hz
Current => 5A
It doesn't need to be precise for the measurement, use the voltage divider is ok.
BR
Kevin