Other Parts Discussed in Thread: TLV7021, TLV7041
Hi Team,
I'm working on a Ti design and I'm looking for a simple and low-cost comparator that has the Open Collector features? Thanks.
Regards
Sean
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Paul,
Thanks for the reply.
+5V power rail;
No specialsupply current spec, low iq that should be better;
Output pull up to power supply;
Normal speed, don't need fast speed;
Input volatge range is better from 0V to 5V;
Singel channel with low cost;
package should be small, SOT23 is ok;
-40C to +85 is ok.
Could you recomend a low cost one for me? Thanks a lot.
Regards
Sean