This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please help me to find the suitable current amplifier

Hi Team,

Please help me the find the most suitable current amplifier for my customer.

I(in) = 1mA

I(out) = 100mA

Freq = 60Hz

Voltage = 14V(typical) ; 20V(max)

Thank you.

  • Kane,

    Are the currents unidirectional or bidirectional?

    What is the voltage compliance of the input current? This limits the maximum input resistance that I can use to convert input current to voltage.

    What is the range of output impedance? 

    Is output load floating or is the termination fixed? (if fixed at what voltage)?

    I could not find a part that does this function directly.