Part Number: INA168
Hello, sir
Circuit :
Input - 20-50V LED converter (especiallay, with 120Hz Current noise)
load - LED 70mA - 3A
Sensing R - 60m ohm
RL = 60.4k // 1uF
VCC - 5V
Result :
ILOAD0 - UNIT FUNCTION 50V after 10msec
Output at OUT PIN : It's stable is OK(simulation and real testing)
Question:
I'd like know using large capacitor, 1uF to RL to make to unstable circuit.
Is there a way to check the impact on the satibiliztion of the chip by using a large capacitor at the output?
Thank you, sir,
Have a good time,
I'd like to know that INA168