We are using the following circuit to generate a -10.00 volt DC reference:
The input to this circuit at R71 is 10.00 volts DC. We adjust R155 so that the voltage at -VREF is -10.00 volts DC. At about 20F, the output takes a sudden shift of about 8 to 10 millivolts. The 10.00 volt input stays constant at this time. The output will remain shifted for several minutes and then shift back. This occurs during a temperature test cycle where we change the ambient temperature from room temperature to 0F at a rate of about 2.5 degrees Farenheit per minute. This shift causes a major upset in our circuit operation. We suspected that the problem had something to do with the potentiometer, so we replaced it with a fixed resistor. The problem remains even with the potentiometer out of the circuit. Can you give us some ideas as to what might be wrong?