Part Number: LT1013D
Hi team,
I would like to know if it's possible to supply this opamp with +15V/0V voltages; will it work on that condition?
Thank you in advance.
Best regards,
Adrian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LT1013D
Hi team,
I would like to know if it's possible to supply this opamp with +15V/0V voltages; will it work on that condition?
Thank you in advance.
Best regards,
Adrian
Hello Adrian,
Yes - the LT1013D can be powered by a single +15 V/ 0 V supply, but the input common-mode voltage range VICR and output voltage range VOM will need to be observed with respect to the single supply conditions.
The VICR, Common-mode input voltage range Recommended range at 25°C and +/-15 V supplies is -15 V to +13.5 V. Since the negative supply is replaced with 0 V the VICR range becomes approximately 0 V to +13.5 V. Similarly VOM, the maximum peak output voltage swing with +/-15 V supplies, RL = 2 kΩ and 25°C, is ±12.5 minimum and ±14 V typical. Therefore, with the single +15 V supply, the VOM would be approximately +2.5 V minimum on the low end, and +14 V typical on the high end.
Regards, Thomas
Precision Amplifiers Applications Engineering