Part Number: TLE2022M
Other Parts Discussed in Thread: TLE2022, TLE2021
Hello,
I have a test circuit in which a sinusoidal signal of frequency 2MHz is applied to TLE2022 IN+ via SPDT switch. The switch is used to select amplitude of the 2MHz sine signal applied to TLE2022 IN+. I need help determining the input impedance (resistance, shunt capacitance) of TLE2022, I did not find a direct spec in the datasheet. I know ideally, the input impedance will be infinite but I am worried this impedance can go down for 2MHz input signal if there is significant shunt capacitance.
I tried to get SPICE model for TLE2022 from TI's website but could not open the files in LTSpice. I do not have access to PSpice or TINA. Is there anyway I can open the part model in LTSpice?
Thanks!
- Swantika