Part Number: INA333-HT
Other Parts Discussed in Thread: INA129-HT, OPA2333-HT, INA128-HT,
Hello,
- In datasheet it says- It is not recommended to use a gain <100 for high temperature (210°C) applications [Application Information,page 14 ]. I would like to know if i need to add any extra circuit for using Gain (25~30) at 150°C in my design or this chip will straight forward work for me without any additional circuit.
- Which package has good thermal characteristics JD or HKJ ? for 150°C Ambient Temperature?
Thanks,
Arif