Part Number: ISO124
Other Parts Discussed in Thread: ISO122, ISO224, ISO120,
Greetings!
My problem is: i need to do a simulation, using the Eagle Software, but i don't have the PSPICE model for ISO124U.
I made a research and found anothers components to replace ISO124U, such as ISO120, ISO122 and ISO224.
The problem is, Eagle only read .mdl extension, but in TI website, the extension is .mod, and i can't change to .mdl
So, anyone have a model that i can use ? Especially ISO124U or ISO120 or ISO122U. I'm searching for hours and i can't find a model to make my simulation.
Thanks!!