This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA818: OPA818

Part Number: OPA818
Other Parts Discussed in Thread: TINA-TI

Hello,

Hope someone can help with this.

I have been getting use to using TINA but am having a problem with power measurement:-

I have attached the circuit, if it is run in transient analysis you will see that PM1 measures the instantaneous power of R3, which appears to be ~ 0.2W.

I want to be able to measure the average power. On the net there are instructions:-

Select Analysis/AC Analysis/Calculate nodal voltages from the menu and then click the power meter with the probe. A table is supposed to appear showing effective power among other things which does not show up!

The only thing that does show up is a display of the power near the watt-meter symbol which is 0W which clearly disagrees with the Transient result!

Thanks.

Best regardsOPA818-1.TSC,

Peter

  • Hi Peter,

    change the signal of "VG1" from "Square wave" to "Sine wave".

    Kai

  • Hi Kai,

    Thanks for your response again.

    Hmmm, yes it does now show the power dissipated in the resistor when the source is sinusoidal. However the dialog window showing:-

    effective power ( P )

    reactive power ( Q )

    apparent power ( S )

    phase (  )

    power factor ( cos )

    does NOT show up.

    I can approximate the squarewave with multiplying the 35V x 2^0.5 but the waveforms and the power dissipated is clearly NOT the same as when driven by a squarewave.

    Clearly this is a limitation in the algorithm - Microcap doesn't have this problem. Not sure about other simulators.

    Apparently one can use the post processor to get a more accurate result. Do you know how to use the post processor or any other way to get a more accurate result?

    Thanks.

    Peter

  • Hi Peter,

    I think this an issue because the free TINA-TI version isn't a full version of TINA.

    The post processor is a bit explained in this TI's "stability" learning video:

    Kai