Other Parts Discussed in Thread: INA333, OPA333, TINA-TI
Hello,
My question is in regards to the following post https://e2e.ti.com/support/amplifiers/f/14/t/293906
1. In here Mr. Mock suggested to filter out the signal before passing it to the Instrumentation Amplifier. The cutoff frequency mentioned is 101Hz however with the R value of 7.5KOhm and C value of 10nF, I calculated the cutoff frequency to be 2122.06Hz. Am I doing something wrong?
2. What is the use of R1 and R2 in your circuit diagram, are those the bridge resistor, did you use a quarter bridge configuration or simply voltage divider circuit?
3. What the use of OPA333 at pin5 for INA333, can I just connect pin5 of INA333 to ground directly?
Looking forward towards your reply, I am a novice as far as electronics is concerned. I am trying to implement a quarter bridge configuration using a 5KOhm strain gage and the peak to peak output voltage from the bridge is 100microvolts.