Part Number: INA148
Hello,
Is an input voltage of 15V (between Vin+ an Vin-) allowed if there is no supply voltage? The supply voltage and Ref is on ground.This could happen, if we perform a high voltage test on the board. The INA148 is connected to a voltage divider so that a maximum input voltage of 15V for 60s can be the result during this test.
If the input voltage is 15V and there is no supply voltage connected (or on ground) what are the maximum values for the output voltage?
Best regards
Thomas