Other Parts Discussed in Thread: THS4551, TINA-TI
I download the reference from ti website THS4551DGK TINA-TI Model (Rev. B) and open the tsc file, the save the macro as (pspice) cir file. Then I simulate the circuits in cadence virtuoso 6.1.7,but cadence simulator spectre report the error during initial setup. The reported error is tb.I0.X_THS4551.R_NOISELESS: 'trise' is too negative, making the model temperature less than 0 k. I post the photo here.
Also I try the THS4551 TINA-TI Spice Model (Rev. B) model file, the same error was reported.
With the same circuit, when I used old model ( released on 07/14/2016, version 1.0) which I also download from TI website. The circuit is simulated smoothly. Can you help me on this? why the lastest model doesn't work with cadence virtuoso?
Some basic information of the old model is listed below for remembering.
*
** Released by: WEBENCH(R) Design Center, Texas Instruments Inc.
* Part: THS4551
* Date: 07/14/2016
* Model Type: All In One
* Simulator: TINA-TI
* Simulator Version: 9
* EVM Order Number: N/A
* EVM Users Guide: N/A
* Datasheet: July 2016
*
* Model Version: 1.0
Thanks,
Morris