Part Number: LMH7322
Other Parts Discussed in Thread: TINA-TI
Hello,
we use the LMH7322 with the following supply voltage:
VCCI +5V
VCCO +2.5V
VEE -5V
We dont need the Latch feature, so we connect the #LE Pin via 10k to VCCO (2.5V).
My question: Is it allowed to connect the LE Pin via 10k to GND (0V), or must we connect the LE Pin via 10k to VEE (-5V)
At the Tina-Ti simulation it runs with LE via 10K to GND.
Kind regards
Jens