The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2140: OPA2140 has abnormal output current when used V/I conversion

Part Number: OPA2140

 Hello,

Our customer used OPA2140 as 0~24mA current source, there is no problem during simulation, but actually, he met a question using PCB to test.

1) single 12V  power supply,  0~2V input, and output 0~24mA, there is no problem.

2) When +-12V power supply, there is 0.25~3mA increasement . For example, 1V input, its output is about 10.3mA instead of 10mA. This phenomenon is appeared when 1~2V input. In addition, the output current could only to 18mA and couldn't increase. 

Could you please give some suggestions? Or if is there some pcb layout issue? The circuit is as following:

 

Best regards

Kailyn