Part Number: TLC3704
Dear expert(s):
The TI datasheet for TLC3704 specs an absolute maximum input current of +/- 5mA. That, of course, applies to the part when it is powered.
During a Flying Probe test of a transient voltage suppressor connected to a TI TLC3704 IC by a resistor, inputs of this device may experience a pulse of 5mA, of either polarity, for 5ms, while the part is unpowered. Since this test is on an avionics flight module, and practically everything gets a high-level review, it would be helpful to have an official statement from TI that states that not only would a 5ms pulse of either polarity be non-injurious to an unpowered TLC3704 IC of any-grade, but a 5mA pulse applied for some longer time (such as 10ms, 100ms, or 1s) would similarly be non-injurious.
The best statement would be this: "No stress or damage would be caused to an unpowered TI TLC3704 IC of any grade by applying, to any one of its inputs, a continuous current of 5mA of either polarity with respect to its negative-supply terminal (pin 12 in the package used in this assembly)."
We'd be grateful for such a statement. Please advise us on this matter.
Thank you.
Ed Riess