Part Number: OPA376
Hi TI experts,
I met an issue when using OPA376, circuit is configured as below:
Supply voltage is 3V and GND, Vref is 400mV. signal source VG1 is a normal sine wave with hundreds of uV level.
when I connect voltage source J_P and J_N to J_PRE_P and J_PRE_N, the measured signal (VM) is like this: seems half of the sine wave is moved up and down.
while when I remove the first stage OPA376 (IOP1 and IOP2 in figure above), and only use the second stage OPA376 (IOP3 and IOP4 in figure above), with J_P and J_N connected to J_POST_P and J_POST_N,the signal becomes normal and no distortion:
This really confused me. What lead to the distortion when I add first stage? is it because
(1) offset? but OPA376 is also used in the second stage, why no distortion appeared?
(2) crossover? but why the second stage doesn't have crossover distortion?
any other possible reasons? how to explain this?
Thanks!
LZ