Part Number: TL3474A
Other Parts Discussed in Thread: TL3474, TL3472
I'd like to know the common mode input range for TL3474 when VCC+=18V and VCC-=0V. What's the minimum input common mode voltage? 0V or ?Thanks.
Regards
Brian W
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Brian,
The term single supply (in the device title) means that input range includes the negative supply rail so that rail can be grounded. It also means that the output range gets close to ground but maybe not all the way. TL3472 VOL is typically 0.1V with a 2k load to ground. The TL3472 actually fights the 2k load a little bit.
Minimum input range will be 0V
One more question, With configuration of the single supply by 0Vdc(VCC-) to 18Vdc(VCC+), once VCC+ is up to 20Vdc, what happens? Can the device be damaged by over voltage? If not so, what's the allowable max. VCC+? 36V? Very thanks !
Regards
Brian W
Brian,
Kai's suggestions are correct. V- = 0 with V+ = 18/20V will work fine all the way to V+ = 36V.
And again, make sure your input voltage is within the recommended range for normal operation and within the absolute maximum range to avoid damage.
Regards,
Daniel