We use the internal temperature sensor of the PGA309 in the signal conditioning circuitry of a pressure sensor. The external EEPROM is loaded with temperature correction coefficients which the PGA309 indexes to correct for temperature errors.
In a controlled oven at cold temperature, when full scale pressure is applied to the sensor, the output of the PGA309 is slowly moving. We have tracked this to movement of the internal temperature sensor. The temperature correction is fairly large so a small movement of the temperature sensor causes noticable/unacceptable movement on the output of the transducer. The temperature sensor reading moves about six degrees celsius in the first two minutes that pressure is applied. The temperature sensor does not move when no pressure is applied.
Why is the temperature sensor moving and is there a way to stop it from doing so? Please note that the temperature of the sensor and electronics are stable and the temperature sensor does not change when no pressure is applied to the sensor.