Part Number: LMH6552
Other Parts Discussed in Thread: LMH5401
Hi,
I need to deliver a single ended signal with 2.8 VPP amplitude to 1 50 ohm load. The frequency of the signal is ranging between 100 to 700 MHz. I have decided to go with LMH6552 as it has a bandwidth of 1.5 GHz with voltage swing of 10 V. I have designed the LMH6552 for gain of 5V/V. I have attached my TINA file. Could you please let me know why for frequencies above 200 MHz the output signal is not sinusoidal anymore?
Please kindly note that I can provide either differential or single ended signal to the LMH6552 but the output should be single ended.So I appreciate if you let me know if there exist any better TI product for this application.
Regards
SamanehLMH6552.TSC