This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

long term gain drift of the INA132

Other Parts Discussed in Thread: INA132

A customer is asking the following question about the INA132.

 

Can you get me data on long term gain drift of the INA132? Not pass/fail test data but real measurements? I need to estimate system 1 year accuracy and make recommendations about how often to recalibrate to stay within specs.

 

Thanks,

  • Hello Roger,

    All long-term stability specs are guaranteed by a life-test during the initial introductory phase of the project when a large sample-size of the new parts undergoes accelerated aging process in high temperature ovens.  The life-test simulates (or is equivalent to) 10-year aging process and the shift of various parameters during the life-test is used to set the maximum guaranteed specs at room temperature. 

    Here are the gain specifications from the PDS:

    For the INA132PA, the initial error is +/-0.1%.  In addition to that, you will need to add 1/10th of the maximum error to approximate 1 year of shift.

    You need to keep in mind, however, that the long-term shift is not quite linear - it is steeper in the fist few years and slower in the later years and it usually excludes first month due to continuing self-curing of the molding compound used for packaging