Part Number: LMH6702QML-SP
Other Parts Discussed in Thread: LMH6702, THS3217, THS3215, VCA820, OPA695, THS3491, OPA683, OPA684
We are using the LMH6702 for an aerospace application and would like to achieve the best CMRR available. I understand one of the demerits of CFAs is poor CMRR compared to VFAs but the typical performance curves on the datasheet indicate 20dB at 100MHz and over 40dB at 10MHz. While these may not seem it would be beneficial to our design if they could be achieved.
I have two questions:
1) can you provide the test circuit used to perform the CMRR measurement for this part?
2) Can you recommend design strategies or methods to optimize the available CMRR?
Thanks in advance for any guidance you can provide.
Best regards,
Chris Belting