Part Number: XTR106
Hello,
I am designing a circuit for load cells using XRT106. The circuit is based on the FIGURE 1. - Basic Bridge Measurement Circuit with Linearization from the XRT106 datasheet.
The resistors R1 and R2 form bridge trim circuit to compensate for the initial accuracy of the bridge, what means it adjusts 4mA @ 0.0000mV/V (or unbalanced load cell ZERO).
R1 is a fixed value resistor and R2 a trimmmer resistor (trimpot).
Vin is connected before R1, what means R1 does not affect the load cell SPAN.
For example, a standard 1kg load cell with 2mV/V output: zero=0.0110mV/V and Span 1.9890 mV/V. The ZERO value can be adjusted using R1 and R2 resistors to balance the bridge, to result in 4mA output. What means that 0kg on the load cell is 4mA (0.0110 mV/V adjusted to 0.0000mV/V).
I did not figure out how to adjust the Span for any type of load cell. For this specific load cell, I can calculate RG for VFS 1.9890mV/V to give me 20mA @ 1kg of mass?
I would like to use another trimmmer resistor to adjust SPAN (20mA). Would I use a trimmer resistor on RG? What would be the best technique to adjust the SPAN?
Thanks in advance,
Márcio Cabrini