Other Parts Discussed in Thread: AMC1200
Hi Support team,
I connected LEM LV25P voltage sensor and AMC1200Q1 for voltage measurement.
I have two power supplies each has 4 channels, one DC power supply is for LV25P (VCC1, VCC2, GND1), and the input side of AMC1200 (VDD2, GND2, the other one is for the output side of AMC1200 (VDD3, GND3).
I obtained +15, -15 and GND1 using two channels of the power supply as in the figure. The input of LV25P is 100V AC sine and there is a measurement resistor in the output (R1 22). As I know that the input of AMC1200 is differential and so I measure differential voltage using AMC1200. One of R1 pin is connected to GND1 and VINN pin of AMC1200, the other pin of R1 is connected to the output of LV25P and VINP pin of AMC1200 as in the attached figure. I set up the experimental model of the circuit.
GND1 and GND2 come from the same DC Power supply,
First, I connected to these common pins as in the picture. I measure the differential rms voltage of the output (VOUTP-VOUTN) using a multimeter, and also I used math function of the oscilloscope to get the differential voltage (CHN1-CHN2). The results are the same, there is no problem.
Second, I connected to GND1 and GND2. The results are the same as in the first scenario.
My question is, should I connect GND1 and GND2 to each other or they should be separate. Because ı will make PCB circuit, before it, I want to be sure about these connections.
Looking forward to your help folks,
Best regards,
danien.