Part Number: LM321LV
Hi,
I am planning to use LM321LV in my design. anybody please tell the output voltage swing level for V+ = 3.3V and V- = ground.
Regards
Dinesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Dinesh,
If the load is low current then swing would be very close to 0V to 3.3V. See figure 6 in data sheet and imagine that -2.75V is actually 0V and +2.75V is actually 3.3V. For higher output current, the output resistance will cause some voltage loss. Again refer to figure 6 and expect a somewhat larger slope because supply is 3.3V instead of 5.5V