This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High Bandwidth differential amplifier/attenuator

Hi Team,

I am looking for differential ampplifier or attenuator to converter a 15V diifeernetial input signal (can be connected to both the input termianls of Opamp) in to a 1.5 V output signal to drive a 50 resistive load. the bandwidth requirement is atleast 25 MHz.

Could you please advice a right opamp.

Thanks