Part Number: XTR111-2EVM
Other Parts Discussed in Thread: XTR111
Dear Sir,
Many thanks for the suggestion, I could use the TINA simulator and changed some values of the schematic
please see the attached the changes are R 10 = 90 k, V1= 3V (as this is internally set to 3V in XTR111), added R1=10k, R2= 5k to get 4.5 volts at REGF
I could get the output of 4 mA to 20 mA with an input of 0.5 to 4.5 VDC , kindly verify and confirm this is correct
with best regards
K. Ganapathy