Other Parts Discussed in Thread: TL431
Hi Team,
Customer is asking which op-amp do we suggest for the M-BUS ?
From below info, max voltage is 32V, max current is about 2x mA.
Thanks!
Andrew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TL431
Hi Team,
Customer is asking which op-amp do we suggest for the M-BUS ?
From below info, max voltage is 32V, max current is about 2x mA.
Thanks!
Andrew
Hello Andrew,
M-Bus, that I only have known about for 10 minutes from one page description, is a digital system so starting with the op amp is not a great plan of action.
The power supply is a better place to start. I would think that a 1.3mA current source that charges a capacitor to an under voltage lock out level then enables a low current (1mA) switching supply that output 5V (or less) to run the sensor and logic and op amp. Maybe there is a dedicated M bus power chip available that does this, I have not looked. If the whole module is very low current then a linear regulator (such as a TL431 shunt) could work.
The digital output is a low tolerance 11mA to 20mA , A simple NPN transistor sink driven by logic could do that.
If the sensor needs an op amp, then give the details for that need.