This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA-TI: Fail to create a macro and encounter convergence problem or irregular circuits

Part Number: TINA-TI
Other Parts Discussed in Thread: REF6050

Hi TI experts,

I am using TINA-TI simulating circuits and I have encounterred several problems.

1. I want to simulate an LED driver driving SFH4713A. However, I failed to create a macro using the model downloaded from part supplier. TINA-TI shows 'Invalid device. Line:#20. The circuit cannot be opened or cannot be converted to a macro.' Please find the attached .lib file below. How can I solve this problem? Attaced is the .lib file.

OSRAM-IR-OSLON.lib

2. I cannot create a macro for part REF6050 using the .lib file downloaded from TI. Attaced is the .lib file downloaded from TI.

ref6050 spice model-sbom994.zip

3. In order to simulate a more realistic situation, I prefer to include decoupling capacitors in schematics, as shown below. In addition, I insert am ampere meter in the current loop. However, TINA-TI usually encounters 'Convergence problem' or 'Irregular circuits' so that I have to abort simulation. How can I solve this problem? Attaced is the .TSC file.

SNOM619A-LMG1020 TINA-TI reference design.TSC