Part Number: INA302
Other Parts Discussed in Thread: INA303
Hi team,
Could you help review the INA302A2 schematic and provide your comments? Thanks!
Common mode voltage= 24V
Alert trip point= 20A with 1ms delay
Best regards,
Sam Ting
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Sam,
I see a few issues. First you must attach a reference to the REF pin. If you are doing uni-polar current measurement I would suggest connecting to GND.
Next you have to alarm conditions connected in a configuration that if the current is above either condition then the output is low. Were you trying to use the Window comparative version (INA303)? As seen in Figure 44 in the datasheet?
The way this is setup the alarm will hit at 6.52A according to my simulations which will include offset and other errors, 6.4A is the calculated value. I have attached the TINA file. I added resistance on the pins so that I can visually see when either one or both Alert pins are active.INA302A2_e2e.TSC
Also your calculated value for the capacitor is incorrect. The value for 1ms should be about 4.1nF. Please verify your calculations and use the equation #2 in the datasheet and Vth = 1.22 and ID = 5µA.
Please verify my suggestions and I could verify your revised design.