Other Parts Discussed in Thread: LMX2594, , TRF37B75, TRF37B73, TRF37C73, TRF37C75, TRF37D73, TINA-TI
Hello:
I'm working a low noise synthesizer development using the LMX2594 fully integrated synthesizer, and the LM2490 with low noise external VCO's, locked against a very low noise 100MHz reference.
With the resulting low phase noise, a possible issue is the "phase noise" of the buffer amplifiers. Texas Instruments makes a very nice family (the TRF37 line) of moderately low noise buffer amps at frequencies up to 4GHz and 6 GHz with the convenient feature of gains available over the range of 12dB, 15dB, 18dB, and 20dB. The 15dB and 18dB gain parts also come in two power levels, so are convenient for sometimes saving DC power. These parts and major specs are shown in this table:
Part |
Gain |
Noise Fig |
Freq |
Supply, P1dB |
Cost |
TRF37A75 |
12dB |
4dB |
40-6000MHz |
5V/80mA/18dBm |
$0.52 at 1k |
TRF37B75 |
15dB |
3.8dB |
40-4000MHz |
5V/85mA/17.5dBm |
$0.52 at 1k |
TRF37B73 |
15dB |
4dB |
1-6000MHz |
3.3V/52mA/15dBm |
$0.43 at 1k |
TRF37C73 |
18dB |
3.5dB |
1-6000MHz |
3.3V/55mA/16.5dBm |
$0.43 at 1k |
TRF37C75 |
18dB |
3.5dB |
40-4000MHz |
5V/85mA/19.5dBm |
$0.52 at 1k |
TRF37D73 |
20dB |
3.2dB |
1-6000MHz |
3.3V/63mA/16.6dBm |
$0.43 at 1k |
Nice performance at low prices. The only issue with using these as low noise synthesizer buffers is that the "phase noise" is not specified. This is the noise close to the carrier that results from the low frequency flicker noise of the devices mixing up around the RF carrier to create a phase noise like total noise. The parts are SiGe bipolar, which tends to have a low flicker noise, but it is not specified. It could easily be a problem for buffering ultra-low noise crystal references, and possibly ultra-low noise synthesizers as well.
Whatever the noise is, it has to be lived with since there is not any way I am aware of to reduce it through external means. With a discrete transistor buffer, this noise can be reduced through emitter degeneration. To my knowledge, no such options exist for this part.
Has Texas Instruments ever measured this noise? If not, could it be measured?
A discussion of this noise and how it is measured is at:
https://www.markimicrowave.com/blog/how-do-amplifiers-affect-signal-phase-noise/
A detailed article by phase noise expert Enrico Rubiola is attached.
Thanks,
Farron