Part Number: INA226
Other Parts Discussed in Thread: INA229
Dear expert,
My customer is looking for a solution in LED controller to sample the voltage, current and power. Here are the spec they need:
- Supply power is 3.3V
- Voltage measurement is 24VAC(50Hz) and 12V/24V/48VDC
- Current measurement is 10A
- Low side sensing
- Sampling error<1%
- Temperature range is -30~70C
- Load is ADC
They are fine with sampling voltage¤t then calculate the power. However they prefer to IC that can directly sample the power of AC. Please share your solutions and related materials, thanks!