Other Parts Discussed in Thread: LM358
Dear Sir:
I have done circuit experiments on LM385(SOIC-8) and LM385N(PDIP). The schematic diagrams are shown as,
I use power of 5V with amp meter to record their currents.
In LM358N(PDIP) circuit, the current shows 0.7mA and holds for hours.
In LM358 (SOIC-8) circuit, the current begins with 0.7mA same as LM358N,
but a few minutes later the amp meter shows unstable fluctuating value around 25mA to 55mA.
Can you give me some points of difference between LM358 and LM385N.
Best Regards