This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1100: AMC1100DUBR

Part Number: AMC1100


Hi,

I'm using AMC1100 analog isolator for current sensing application.

input side of the amplifier is connected between 5V and ground_1 and output side is connected between 3.3V and ground_2.

there is a voltage difference between ground! and ground_2

ground_2 is 70V above ground_1

Will AMC1100 work is such a configuration? what are the points to consider?