Part Number: OPA2209
Other Parts Discussed in Thread: OPA209, , TINA-TI
I was using Tina TI to build a filter circuit using the OPA2209. I used the macro in the Tina library and my circuit was working fine. I was on line and I noticed a new PSpice file for the OPA2209 called OPA209. I downloaded the file and imported the Macro. Now when I analyze my circuit (transient analysis), it has a 1.5vdc offset (not good). So, I my question is, did I do something bad when I imported the file? Also, when I used the Macro, it came up with an error in which the very last line had a ".P" in it. Tina, did not like that apparently, so I made it a comment. After I did that, the macro came to life and I could analyze my circuit.
I did this with several op amps. If I use the one in the library, it works. If I use the PSpice model you provide and import it, I get the error and the offset. What am I doing wrong.