Other Parts Discussed in Thread: OPA381, OPA350, OPA340, OPA380
Hi,
I would like to create a courent source which could provide 25 mA as constant output current. I read the datasheet(OPA381) and it says that the current typ is 10 mA. I couldn't find how much is the ouput current max. I already have the schematics of my circuit that include an Amplifier. I would like to know what Operational amplifier Low power could support 25 mA as output current?
Thank you for taking time.
Steven