Hi
LM2902 TINA simulation: differential circuit.
1. resistor=10k, single 15V power, output is good.
2. resistor=1k, single 15V power, output is wrong.
3. resistor=1k, +15V and -15V power, output is good.
what's the cause? thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
LM2902 TINA simulation: differential circuit.
1. resistor=10k, single 15V power, output is good.
2. resistor=1k, single 15V power, output is wrong.
3. resistor=1k, +15V and -15V power, output is good.
what's the cause? thanks.
Max,
The output must be able to sink the current from the inverting feedback. With both input sides at 1.4V , the ideal output would be 0V. With 10k resistors, the feedback current is 1.4V/20k = 70uA . The model supports this sink current at low voltage, however most LM2902 will need to use the second sink driver, a PNP follower, so output will be near 600mV. With 1k resistors, things get worse; now sink current is 700uA so an output near 0.7V is certain. See figure 1 in data sheet, output sinking characteristics. Also see application note section 3.1 , Design Guidelines for Devices with LM324/LM358 Cores
Try 100k resistors, that is only 7uA sink current.