Hi I cannot determine from the datasheet if the INA226 Vbus pin is always loading the rail being measured at the pin, irregardless of whether or not it is measuring Vbus, or is it switched in or out depending upon whether or not the device is measuring Vbus voltage or shunt voltage? It seems to imply that the amplifier is always connected and that the ADC is switched to the Vbus amplifier as required, but wanted to verify that this is the case.
Also the datasheet specs a typical value for the Vbus impedance of 830 kohm, but no min/max values are supplied. What is the range of impedance values?
Thanks.