This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Where is "the online calculator tool on the INA226 product page for this purpose as well. "?

Part Number: INA226


Hi where is "the online calculator tool on the INA226 product page for this purpose as well. " mentioned in this case? I can't find it on the page. Thanks.

  • Hello N,

    Unfortunately the error calculators were taken down by mistake from our digital current sensor pages. We are aware of the issue and working to get them restored as quickly as possible. I apologize for the inconvenience.

    In the meantime, I am happy to assist you with a particular error calculation if you provide me with the circuit conditions.

    Best regards,

    Ian Williams
    Applications Manager
    Current Sensing

  • Hi Ian thanks. How is the gain error for INA226 calculated? It is listed as 0.1% or 1/1000th, but how is the gain determined for it? Assuming perfect 2 ohm sense resistor (40.96 mA FS). Thanks.

  • Hi N,

    The gain error is calculated the same as for an analog output device, but looking at output register codes instead of output voltage. To test this, two different known differential input voltages are applied, for example 10mV and 50mV. The shunt voltage register is read at each level. The results are compared to the ideal, from which we can determine both offset and gain error using the standard first-order linear equation: output = gain * input + offset. 

    Since there is no gain stage in the INA226, these errors are caused by non-idealities in the ADC and input sampling network.

    Best regards,

    Ian Williams

  • The error tools have been reinstated for the digital power monitor products - including the INA226.