Part Number: TLC2201-SP
Other Parts Discussed in Thread: TLC2201AM
Radiation data for TLC2201-SP is currently unavailable.
Are there any plans to make this data available?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLC2201-SP
Other Parts Discussed in Thread: TLC2201AM
Radiation data for TLC2201-SP is currently unavailable.
Are there any plans to make this data available?
Hi Gregory,
The device marking, 5962-90882 03V2A, is decoded as device type 3 (TLC2201AM), device class V (space application), LCCC 20 package.
In the "SMD" document, section 4, available under "Technical Documentation" on the product page (emphasis added by me) -
4.4.4 Group E inspection. Group E inspection is required only for parts intended to be marked as radiation hardness assured (see 3.5 herein).
a. End-point electrical parameters shall be as specified in table IIA herein.
b. For device classes Q and V, the devices or test vehicle shall be subjected to radiation hardness assured tests as specified in MIL-PRF-38535 for the RHA level being tested. For device class M, the devices shall be subjected to radiation hardness assured tests as specified in MIL-PRF-38535, appendix A for the RHA level being tested. All device classes must meet the postirradiation end-point electrical parameter limits as defined in table I at TA = +25C 5C, after exposure, to the subgroups specified in table IIA herein.
In this case, the part is not sold or marketed as RHA (radiation hardness assured). Hence, these tests were not performed and there is no data available. If RHA is a necessity, the TI Space Products Catalog includes a breakdown of which space amplifiers have RHA versions (see pages 15-16).
Cheers,
Jon